Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

how to establish a communication with M24c32-R?

I am trying to communicate M24C32-R with master but for some reason i could not able to !! It appears to me it might be hardware issue. I have connected E0,E1,E2 to ground , Vcc to 3.3V, WC to ground, I have pulled up SCL and SDA to 3.3V with 10K oh...

Apill by Senior
  • 2819 Views
  • 5 replies
  • 0 kudos

STM704 battery switchover vs UL60950

Hello,We are using two components with unique coin cell backup. The first one is a RTC M41T93SMY6. For this one, I could find AN1011 that states that we don't need external diode and resistor to meet UL60950, it is built in the chip. The second one i...

HLepa.1 by Associate
  • 775 Views
  • 0 replies
  • 0 kudos

Resolved! GPIOB not working in my stm8s003

Hey guys.Im using stm8s003f3p6 and IAR compiler and ST SPL.When i use gpio_init to make pb4 and pb5 output i dont know why the output does not get high and low?Other pins on port c ,a and etc work well.

Dear, we have a problem whith some ST485BDR. When the 120 ohm load resistor is applied, the pin 1 goes to low state, lighting the green RX LED

This board perform 4 channels UART to RS485/422 conversion, using a FT4232 device and four ST485BDR devices. The issue is present in some channels in aleatory way. When I replace the failed ST485BDR device by the MAX485ESA the issued chanel start to ...

RMele.1 by Associate
  • 960 Views
  • 1 replies
  • 0 kudos

2020 STM8 compiler comparison

This is not a question, so it doesn't really belong here, but the community forum is still broken, so there is no other place to post this.I just redid my comparison of the 4 most important STM8 C compilers (previous comparisons were in 2016 and 2018...

Error:stopped on execution protection at 0x800

I used STVD for stm8s105c6 assembly coding. The program compiled and built, since it could not be programmed in STVD, I used STVP for programming, and selected file format of motorola srecord.While, the effect was not I expected. I started to debug, ...

MQi.1 by Senior II
  • 1181 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.