2003-07-09 5:06 AM
2003-06-27 12:30 AM
Hello,
When i mount an 8MHz crystal on my board with 2x 47pF to ground and i switch off the RC-oscillator, the ST7 seems to 'die'. I can't read or write anymore with the ST-Stick and the program doesn't run. When i put the scope on the crystal, the clock doesn't run. Anyone an idea what's going wrong??? Regards.2003-07-01 10:46 PM
What is your device? Did you configure the right oscillator range in option bytes? Which ICP did you choose in STVP7 (OPT disable or enable)?
2003-07-02 12:23 AM
I never used RC-oscillator (not internal nor external) so I'm not sure abuot the following procedure...
I'm programming on ST72324 using inDart. If you use a crystal you should set ''Resonator Oscillator'' in the option bytes. You should program the option bytes when the uC is ''alive'', so: - switch on RC-oscillator - reprogram option bytes with ''Resonator Oscillator'' - connect the crystal and switch off the RC-oscillator In the 72324 datasheet, typical values of capacitors (for a 8MHz xtal) are 33pF each. I hope that can help, Patrik2003-07-02 4:38 AM
Hi,
Programming is OPT enable. Had the problem with the st7lite29 and with the st7dali. I'm using an 8MHz crystall. I choose the 4/8MHz Medium Speed resonator, program this. After doing this (like Patrik told) i switch off the internal oscillator and program the option bytes for a second time. After this the IC died... I must do something wrong but i can't figure out what. Greets2003-07-03 12:32 AM
The signal on the crystal is present only if the option bytes are set correctly. I set two option bytes as follow:
- [OSCRANGE] - Oscillator Range Selection: ''MS: 4-8MHz'' - [OSCTYPE] - Oscillator Type Slection: ''Resonator Oscillator'' Bye, Patrik2003-07-09 5:06 AM
The right way to proceed is the following one:
* as by default, the clock is internal RC, program your Flash * then the option byte (no matter if the quartz is already on the appli board, it will be ignored when configured in internal RC thanks to internal switches): Resonnator oscillator, oscillator mid-range, internal RC off + the other options * remove your ICC cable * make a reset of the MCUWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.