2007-11-19 10:28 PM
2011-05-17 12:48 AM
Dear all,
I'm having probles with downloading and installing CAPS on my new Duo Core lap top PC. The download is fine, but when i unzip and run the install i get lots of errors during installation. I've downloaded the software from another PC also and tried to install this on the orignial duo core machine and this does not work either. It seems the download is fine and bugfree but the unpacking and installing is problematic. On unzipping and running the install i get the following sequence... A box opens up to tell me the program was created by PKSFX for windows. I click on finish and the extraction completes and setup automotically starts. As the setup program runs the following error message is display... The instruction at ''0x7c910f29'' referenced memory at 0xffffffffff. the memory could not be read. Click ok to terminate the program. I then click the ok button and i get another box... Unknown return code 'jtdcfgw.exe' I click ok , this box closes and another opens... Setup is not complete. CAPS is not installed. Any thoughts ? David Giles :oWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.