2007-02-07 9:22 AM
Can someone try this program to make sure it works?
2011-05-17 12:36 AM
I have been unable to get this very simple program to work on an str9:
#include ''91x_lib.h'' static GPIO_TypeDef *GPIO4 = (GPIO_TypeDef*)GPIO4_BASE; static SCU_TypeDef *SCU = (SCU_TypeDef*)SCU_BASE; static FMI_TypeDef *FMI = (FMI_TypeDef*)FMI_BASE; void main() { /* Set the peripheral Clock to MCLK/2 */ /* And main clock to the oscillator */ SCU->CLKCNTR = 0x00020082; // Disable port reset SCU->PRR0 |= 0xffffffff; SCU->PRR1 |= 0xffffffff; // SCU->PRR1 |= __GPIO4; // Digital mode SCU->GPIOANA = 0x00; SCU->PCGRO = 0xffffffff; // Enable GPIO port clock SCU->PCGR1 |= 0xffffffff; // SCU->PCGR1 |= __GPIO4; // Enable alternate output 1 SCU->GPIOOUT[4] = 0x1 << 8; // Push/Pull mode SCU->GPIOTYPE[4] = 0x0; // Output direction GPIO4->DDR |= GPIO_Pin_0; // Disconnect from input SCU->GPIOIN[4] = 0; // Pin value GPIO4->DR[GPIO_Pin_0 << 2] = 1; while(1) ; } The idea is just to set GPIO4 pin 0 to prove it's running. The compilation sequence is: /opt/gnuarm/bin/arm-elf-gcc -O3 -c -I. -Ilibrary -mcpu=arm9 -nostartfiles bootloader.c -o bootloader.o /opt/gnuarm/bin/arm-elf-gcc -mcpu=arm9 -nostartfiles -Tlinker.ld -o bootloader.elf bootloader.o /opt/gnuarm/bin/arm-elf-objcopy bootloader.elf -O binary bootloader.bin The symbol offsets are: 0000000000000000 t $a 0000000040000008 B __bss_beg__ 0000000040000008 A __bss_end__ 0000000040000008 A _bss_end__ 0000000040000000 d $d 0000000000000068 t $d 0000000040000000 D __data_beg__ 0000000000000074 A __data_beg_src__ 0000000040000008 D __data_end__ 0000000040000008 A _end 0000000040000008 A __end__ 0000000000000074 A __end_of_text__ 0000000040000000 d GPIO4 0000000000000000 T main 0000000040000004 d SCU 000000004000fffc A __stack_end__ JTAG shows the flash is programmed correctly. It neither works from primary or secondary flash. The reset pin is high. Only one set of VDDQ, VSSQ, VSS, VDD pins is connected because a continuity test says they're all common. VBatt is disconnected. GPIO4:0 is never affected during execution.2011-05-17 12:36 AM
No-one has a clue on this one. How about an example gnuarm command sequence that is known to work.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.