2004-07-19 3:58 PM
can ''program memory'' and ''option byte'' be saved as one file?
2004-07-15 12:35 AM
Can ''program memory'' and ''option byte'' be saved as one file?
so that I do not need to set option byte again each time I enter ST VP!2004-07-15 2:45 AM
They can but stvp would ignore it. Why do you not just setup a project
Regards sjo2004-07-19 3:58 PM
can open the project aslo load the option byte?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.