2007-11-22 9:39 PM
Can interrupt mode for the STR73x
2007-07-18 10:05 PM
I am using the STR73x, ive tried CAN code in software library and i ve confirmed polling mode works fine, but i failed in interrupt mode. I am not sure if this code does some thing at all. No messages send.
Thanks void CAN0_Demo_Interrupt(void) { CAN_InitTypeDef CAN0Init; CAN0Init.CAN_Mask = CAN_CR_IE; CAN0Init.CAN_Bitrate = CAN_BITRATE_125K; // initialize the interrupt controller EIC_IRQChannelConfig(CAN0_IRQChannel, ENABLE); EIC_IRQChannelPriorityConfig(CAN0_IRQChannel, 1); EIC_IRQCmd(ENABLE); // initialize the CAN at a standard bitrate, interrupts enabled CAN_Init(CAN0, &CAN0Init); // switch into Loopback+Silent mode (self-test) CAN_EnterTestMode(CAN0, CAN_TESTR_LBACK | CAN_TESTR_SILENT); // configure the message objects CAN_InvalidateAllMsgObj(CAN0); CAN_SetTxMsgObj(CAN0, CAN0_TX_MSGOBJ, CAN_STD_ID); CAN_SetRxMsgObj(CAN0, CAN0_RX_MSGOBJ, CAN_STD_ID, 0, CAN_LAST_STD_ID, TRUE); // send a pre-defined data frame (void)CAN_SendMessage(CAN0, CAN0_TX_MSGOBJ, &TxCan0Msg[0]); // reception and release are done in the interrupt handler wait(); // switch back into Normal mode CAN_LeaveTestMode(CAN0); // disable interrupts globally EIC_IRQCmd(DISABLE); }2007-11-22 9:39 PM
Does it work at the moment? I am trying to get it work myself but so far no good result. I am used to work with NXP and I think ST didn't document it all so well. Very hard to find what I am searching for. I prefer to write my own values to the registers not to fill in some functions in which I don't know exactly what will be set and what not.
You can also contact me at basvandijk86[at]gmail[dot]comWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.