2004-02-22 11:23 PM
2004-02-22 6:08 PM
Can anyone see a bug in this code which would allow the stack pointer to be modified?
ROM:8A30 WRITETOEEPROMX: ; CODE XREF: WRITEATOEEFROMX+9j ROM:8A30 ; WRITEATOEEFROMX+Ej ... ROM:8A30 83 trap ROM:8A31 CD 82 23 call ENABLEINTERRUPTS ROM:8A34 AD 0D callr KILLWRITEOKBITS ROM:8A34 ; End of function WRITEATOEEFROMX ROM:8A34 ROM:8A36 ROM:8A36 ; ¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦ S U B R O U T I N E ¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦¦ ROM:8A36 ROM:8A36 ROM:8A36 EECONTEXTRESTR: ; CODE XREF: WRITEATOEEFROMX+17p ROM:8A36 ; WRITEATOEEFROMX+1Cp ... ROM:8A36 B6 72 ld a, EESAVERCADRH ROM:8A38 B7 4A ld RC1ADDRH, a ROM:8A3A B6 73 ld a, EESAVERCADRL ROM:8A3C B7 4B ld RC1ADDRL, a ROM:8A3E B6 70 ld a, SW1 ROM:8A40 BE 71 ld x, SW2 ROM:8A42 81 ret ROM:46A0 SMOD3JMPXA: ; CODE XREF: SETUPBLOCKOUT+1p ROM:46A0 3F 5E clr NUMINFOBYTES ; Init # bytes in info field ROM:46A2 3F 5F clr INFOFIELDPTR ; Init pointer into info field ROM:46A4 CF 01 A5 ld SELDMOD3_01, x ; Save address of routine that will ROM:46A7 C7 01 A6 ld SELDMOD3_02, a ; build the output message ROM:46AA A6 5A ld a, #$5A ; Get a JMP $XXXX instruction ROM:46AC C7 01 A4 ld SELDMOD3_00, a ; at SELFMOD3 ROM:46AF 3F 61 clr MSGOUTPTR ; Clear pointer to current byte # ROM:46B1 05 50 0A btjf FLAGS0, #2, loc_0_46BE ROM:46B4 CD 46 0C call BUILDMSGFROMSM3 ROM:46B7 10 0B bset UARTREG, #0 ROM:46B9 CD 82 23 call ENABLEINTERRUPTS ROM:46BC 9A rim ROM:46BD 81 ret ROM:46BE ; ---------------------------------------------------------------------------2004-02-22 11:23 PM
Hi!
Can you check your stack depth at each of your calling function, for example check at ''call ENABLEINTERRUPTS'' and so on, because if your stack size is nearing the limit and if you are using the stack(i.e. calling function), then it may cause a problem. Also check the no of called functions inside a function. Like if function1 calling function2 and this calling function3 and so on. --KrselWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.