Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

M95P32: Missing RAM block in the Block diagram

Hi,Why is there no RAM block inside the Block diagram?In the document AN5747 (Page EEPROM memory architecture) there is a RAM block mentioned, but in the block diagram from the M95P32 datasheet no RAM block is available/visible.Thanks in advancenobod...

nobody_0-1719838574624.png
nobody by Associate II
  • 1717 Views
  • 2 replies
  • 0 kudos

M95P32 page write behaviour

Hi,Why is the page-write consuming less power then a page-program? When I understand it correctly then the page-write, is first erasing the page and then writes the values back. So then the page-write power consumption should be similar to erase and ...

nobody_0-1719815321417.png
nobody by Associate II
  • 989 Views
  • 0 replies
  • 0 kudos

Z85C30 SDLC Communitcation issue

I am setting up SDLC communication using the Z85C30 chip. However, when I enable Tx and send data, it appears that the data is mixed with 7E. After the Tx is finished, I disable it. Is there a way to ensure that 7E appears only at the start and end?

Dlak by Associate II
  • 1833 Views
  • 3 replies
  • 0 kudos

Can't get stm8s003f3p6 to work with LCD1602!

Hello there! I am trying to get an stm8s003f3p6 to display text on an LCD1602 the LCD has the adapter board PCF8574 on it.I'm using STVD and cosmic C compiler. I used chatgpt to write the code and after quite a bit of tweaking i got it to compile and...

PCF8574-IIC-I2C-TWI-SPI-Serial-Interface-Board-Top.jpg
ram80 by Associate
  • 1454 Views
  • 1 replies
  • 1 kudos

Learning materials to improve the code

I'm Intermediate in Embedded C and I need to improve my code's readability, safety, scalability and portability with designing a software architecture. Can someone suggest good learning materials (books or courses) where I can learn these.

jsw2000 by Associate II
  • 1034 Views
  • 0 replies
  • 0 kudos

EEPROM - M24M01E-FMN6TP

Hi, We have made a custom development board integrated with M24M01E-FMN6TP EEPROM IC. It is operating at 1.8. Having queries like whether the supply voltage plays a role in accessing total pages of EEPROM and if so please tell us the minimum voltage ...

Resolved! Failure rate (FIT) of BAT30SWFILM

Hello,Can someone provide me the failure rate (fit) of this Schottky diode? I'm updating our database and couldn't find this information on any datasheet / report.PN:  BAT30SWFILMIf the number isn't available could someone provide a guide of how to c...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.