2026-03-03 12:51 AM - last edited on 2026-03-03 5:14 AM by Peter BENSCH
Hello STM Support Team,
I am currently using the ADC1283 to acquire analog data with the PIC32MZ2048EFH100 microcontroller via SPI.
I have verified that the MCU’s SPI module works correctly when tested independently. However, when interfacing with the ADC1283, the device is not returning valid conversion data and consistently responds with 0xFF.
At this point, I am unsure whether the issue is hardware-related or software-related. I am sharing the following for your review:
Firmware source files (.C and .H) (I referred one of your example firmware for ADC1283 from any online portal and created logic).
SPI configuration details
Schematic diagram
Could you please review them and help identify the root cause of the issue?
Our project is currently in the testing phase, so resolving this issue is quite urgent. Your prompt support would be greatly appreciated.
Thank you in advance.
Best regards,
Tushar
Solved! Go to Solution.
2026-03-03 7:52 AM
I think you have SDI and SDO reversed, SDO should go to Din.
2026-03-03 5:14 AM
Unfortunately, you only attached ‘hardware Schematic1.jpg’ with a practically illegible 96dpi, so that neither the type of level translator nor its device number (Uxx) can be read. If it is one of the suspected TXS0104 or TXB0104, please check whether you are controlling OE correctly: typically, SS is low-active with SPI, but the level translator works in reverse.
Regards
/Peter
2026-03-03 6:32 AM
I am using TXS0104EQPWRQ1 level translator. I am attaching the schematic in pdf format for batter resolution.
I also tested the voltage of CS pin from both the site during CS high and low condition. it changes the voltage level properly.
as per the datasheet the OE pin is only for enable and disable the TXS0104EQPWRQ1 level translator.
Best regards,
Tushar
2026-03-03 7:33 AM
Thank you for the PDF, before it looked to me as if OE was controlled by SS.
Have you tried controlling U9 directly instead of through U12 (of course supplying U9 with 3.3V instead of 5V)?
2026-03-03 7:52 AM
I think you have SDI and SDO reversed, SDO should go to Din.
2026-03-06 6:29 AM
Hello Chris, @Peter BENSCH
yes, this is a good observation.
I swapped the SDO and SDI and tested.
Now ADC is working and providing data through the SPI.
Thanks for providing solution.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.