Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Does the an2781(software uart) must use the tx

Posted on October 10, 2011 at 03:26I found if i disable the SWUART_TRANSMIT_USED ,it will hang in TIMERx_UPD_OVF_BRK_IRQHandler and can not run out of it. In this function: #ifdef SWUART_TRANSMIT_USED  uart_Tx_timing(); #endif  The clear_owerflow_fl...

cgh21 by Associate II
  • 1434 Views
  • 3 replies
  • 0 kudos

Beginner

Posted on July 23, 2011 at 10:38Hi All, Yesterday i just got stm8s-discovery board.I don't know how to make use of it to the max since i am unaware about the compiler used with stm to build the code and other info regarding STM, till today i am fami...

TSL 2.4.0 STM8S105C6 on GPIOE not work in IAR

Posted on October 05, 2011 at 18:29if stm8_tsl_conf.h select GPIOE:#define SCKEY_P1_PORT_ADDR  (GPIOE_BaseAddress)  /**< Single channel key Port 1: GPIO base address */ IAR stopped on - ''__iar_unhandled_exception''

prc by Associate
  • 1082 Views
  • 2 replies
  • 0 kudos

STM8L discovery kit ( using raisonance ) error

Posted on October 09, 2011 at 07:29Hi all , I have try to compile default code ( discovery demo ) and everything runs fine. After which i try to create my own application following the guide : UM0991 <Building, debugging and running your applicatio...

lau by Associate
  • 952 Views
  • 1 replies
  • 0 kudos

STM8 Assembler using STVD

Posted on September 18, 2011 at 19:13I use STM8 Assembler. Code: ...... CLOCK EQU 16000 TIME EQU CLOCK/1000 .... compile error Error 67: Improper Character(s) '/1000' Why? I find :) TIME EQU {CLOCK/1000} Works without errors

Problems debugging with STVD

Posted on November 13, 2010 at 07:52Hello, I am unable to debug on the STM8L-Discovery using STVD, I always get this error when trying to start a debug version: Connection error (usb://usb): swim error [30004]: comm timeout I tested STVD versions 4....

SPI slave communication

Posted on September 21, 2011 at 00:02Hi all,I am working a project that has a SPI master on an OMAP-L138.  I had the four lines manually wired across from the OMAP-L138 to the STM8-S discovery board.  The connections are below:OMAP SPI CS -> STM8 SP...

ttran by Associate
  • 748 Views
  • 0 replies
  • 0 kudos

Cosmic linker error - Section Boundary crossing

Posted on September 14, 2011 at 15:24Hi all, I am busy modifying my code so that I can utilize a custom bootloader. My application code is running and compiling with no problems on its own. The problem begins when I try to shift the start address o...

nsayag by Associate II
  • 3032 Views
  • 6 replies
  • 0 kudos

Flash Loader Demonstrator stuck at 82%

Posted on September 16, 2011 at 15:34 Hi, I am trying to download my application using the flash loader demonstrator and I am running into a problem at the same point each time - After 82% of the download the communication stops (see attache...

nsayag by Associate II
  • 978 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.