eStudio,VIPER25
Posted on April 07, 2011 at 07:29Dear friends, I need use the VIPER25, is there anybody working on that. Because eStudio no provision for VIPER25. If any application note also ok for me. #estudio #viper25
Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.
Posted on April 07, 2011 at 07:29Dear friends, I need use the VIPER25, is there anybody working on that. Because eStudio no provision for VIPER25. If any application note also ok for me. #estudio #viper25
Posted on March 05, 2012 at 03:59If it's possible to use LSE as the clock source of TIM1 or TIM2/3/5 or TIM4 ?Use LSE as external trigger of TIM1 or TIM2/3/5 or TIM4 is accepted too, if possible please share some code sample. #stm8-timer-lse
Posted on March 15, 2012 at 05:57I'm trying to get I2C working, I've verified I can manually toggle the pins at 400KHz with a pull up resistor. I can't seem to get the I2C code to work correctly though. input_clock = CLK_GetClockFreq()/1000000; ...
Posted on March 14, 2012 at 13:25I am unable to understand the IAR files involved in developing an application for STM8S103F3. Specifically, the files involved for interrupts and where to write the ISR for the interrupts, when using the IAR IDE. Fur...
Posted on March 08, 2012 at 20:57 Hello, I try measure frequency 50-500Hz. I use STM8S-DISCOVERY KIT with STM8S105C6T6 and FWLib. How initiate the appropriate timer and which port to use? #include ''stm8s_con...
Posted on February 15, 2012 at 20:16Is there any good library to manage the STM8S I2C peripheral running as a slave?I have tested some examples and I'm having many problems in noisy environments, the bus is busy but both slave and master wait for th...
Posted on November 22, 2011 at 16:17hello, I'm trying to trigger the ADC1 with the TRGO signal of TIM1, here is the code that I,m using to configure the timer: TIM1_DeInit(); TIM1_TimeBaseInit(128, TIM1_CounterMode_Up, 62500, 0); TIM1_SelectOutputT...
Posted on March 09, 2012 at 04:26Hello all, I connected crystal 32.768 khz to pin C5,C6 of stm8l151. I want to use RTC-calendar but look like crystal not work. /* Enable LSE */ CLK_LSEConfig(CLK_LSE_ON); /* Wait for LSE clock to be ready */ ...
Posted on December 08, 2011 at 15:57In debugger STVD permanently there are failures. Only reboot helps
Posted on March 06, 2012 at 19:36I want the device to be ''like a virgin''. I've tried STVP but erase option is not visible there. Why?What is another method to erase the chip ? Is that possible to be done by EWSTM8 of IAR ?Thanks,E.L.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.