Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ISB027V1 Firmware

Posted on March 15, 2017 at 11:45Hello,I have a problem with the ISB027V1 Eval.Board. I have flashed and erased the Firmware and now I am looking for the File that is mentioned in the user guide WBC_FW_A11 .... but I cannot find it anywhere. Can som...

CAN bootloader problem

Posted on March 06, 2017 at 23:07Hello! I can't initialize internal CAN bootloader on stm8AF52A8 with HSE 24 MHz, it is silent.I tested all: �bootloader enable� option byte is set.CAN is OK, i tested it in my program.HSE is OK.Soft on PC is OK, I t...

Turns Ratio Notation 'm'

Posted on March 07, 2017 at 15:21HI:I'm using the eDesignSuite to design an AC/DC transformer that has a secondary at 135 vdc, 40 Iavg.  The listed turns ratio is 550.26m .... why the 'm' ?Here are the transformer details:Transformer Specifications:...

STM8L LCD Register

Posted on October 26, 2016 at 11:18Hi, I'm using the STM8L052R8 for temperature measurement, so using an ADC channel, and then displaying the temperature on the LCD.It would be really handy to be able to clear the LCD Ram memory instead of writing t...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.