Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Simple remote control using STM8L001J3

Posted on May 18, 2018 at 11:05Hi, I would like to use the SWIM port of STM8L001J3 to control an LED.Obviously the same port will also need to be used for debugging and programming.I ask if it is possible to connect the LED directly to the port or i...

Failed to set configuration with MCU name STM8AF5289: SWIM error [30006]: Comm init error: chip does not answer

Posted on March 09, 2018 at 10:56ST-LINK Programmer few times its working ,mostly its displaying error messageFailed to set configuration with MCU name STM8AF5289: SWIM error [30006]: Comm init error: chip does not answer connections every thing ok ...

How start learning of stm8S003f3 ?

Posted on February 26, 2018 at 12:00hi  i am kalpesh  , i new in stm8 . I want to learn how to program in stm8. Please tell me which software should i use?please help me . i have Stm8s003f3 20pin IC . i search @ internet i didn't  get ? please help ...

Resolved! STM8S103F3 PC4 problem

Posted on May 14, 2018 at 19:23I am using cheap Chinese board with STM8103F3 chip.I want to use PC4,PC5,PC6 and PC7 pins as inputs connected do keys.With PC5-PC7 there is no problem. I configured them as pull-up input with interrupt, but PC4 is diff...

Timers

Posted on May 11, 2018 at 11:33Hi,I am using  stm8s controller. I am using TIM1,TIM4 for timing delay now i need to use PWM for led blinking. Can i use TIM3(general purpose timer) for timing delay or not , because TIM1(16 bit advanced control timer)...

How to save data in loss of power supply?

Posted on May 15, 2018 at 22:34Hi.I was trying to end my project but I faced a problem.In my project, the user enters a number named IDEAL_TEMPERATURE. But I need that his data won't get lost when the power supply is suddenly interrupted for some mi...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.