Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

we are using wifi module SPWF001A, now we wants to implement the HTTPS secured protocol.But in modules AT command literature ,the commands are for HTTP only. Will HTTP command valid for HTTPS also.

we have completed the prototype functional testing and 150 pilot batch is in progress, before going to mass production(2000 Nos ) we need to implement the security protocol.

VKuda by Associate
  • 1202 Views
  • 1 replies
  • 0 kudos

Slave select and FIFO use on BSPI in STR73x

Posted on June 28, 2018 at 20:06Hello,In my application, I am trying to interface a pressure sensor to the STR73x on BSPI1. The sensor will send pressure information to the STR73x, so the operation is pure receive mode. I have configured the BSPI1 a...

sira rao by Associate
  • 1578 Views
  • 1 replies
  • 0 kudos

Foot print problem with ECMF02-2HSMX6

I have questions about the dimensions of this component: 1. The gap between pins can be questionable. Referring to page11, Gap = E-L1-L2. If I use nominal value, gap is 1.35-0.45-0.75mm = 0.15mm only. If I use the maximum value, gap is 1.4-0.55-0.85...

dvuko by Associate
  • 1246 Views
  • 1 replies
  • 0 kudos

SPWF04SA: product status

Hi,the SPWF04SA is labeled as "NRND" in its product web page. Is there any replacement for it in the roadmap?.In particular, I am interested in WiFi modules supporting Micropython onboard.ThanksRegards

ALM Tech by Associate
  • 997 Views
  • 1 replies
  • 0 kudos

Crashes STVD Develpment tool

Hi, I Install STVD Version 4.3.12 for STM8S Application programming. I used Cosmic Compiler for the same application. But while opening programming in tool menu, STVD is crashes and pop up message " STVD has stopped working". Please find attached...

COSMIC Compiler STM8 Crash

hi,My project used to compile using previous cosmic_32k limited version compiler. It's license got expired on 7th June 2018.After installing new compiler, when i compile, the " cxstm8 program crash " dialog box opens in windows 8.1.then, i have manua...

PWM in STM8S001J3

Hi I have red the reference manual if STM8S001J3, but I still confused whether pwm is the same as TIM ? But when I checked in the section of TIM1, TIM2, adn TIM4... Only TIM1 and TIM2 that have pwm mode. Does it mean that STM8S001J3 only has 2 pwm mo...

How to get STM8 unique device ID?

I'm working with a STM8S003F3P6 microcontroller and I need to know an unique ID for each device I will use. I know that PIC microcontrollers has an unique device ID that can be acessed by the user. My questions is: The STM8 microcontrolers have this ...

Failed to set configuration with MCU name STM8AF5289: SWIM error [30006]: Comm init error: chip does not answer

Posted on March 09, 2018 at 10:37--> While flashing code to stm8  board through ST-LINK/V2 programmer ,i am facing this problem ,it showing message       and unable to flash code , -->ST-LINK/V2 programmer not working properly ,rarely it will work ,...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.