2018-08-06 11:23 PM
hi,
My project used to compile using previous cosmic_32k limited version compiler. It's license got expired on 7th June 2018.
After installing new compiler,
when i compile, the " cxstm8 program crash " dialog box opens in windows 8.1.
then, i have manually executed the instructions to compile my project.
RESULT: It has sucessfully created svk.cx1file.
2. then, "cgstm8 -o\svk.cx2 -l \svk.cx1"
after this instruction, I get "close program" dialog box in windows 8.
It has created the svk.cx2 file, but the file is incomplete. the last few line of the svk.cx2 files are
L176:
.source "test_gsmbase.c:294"
tnz _status
jreq L576
.source "test_gsmbase.c:296"
mov _intra_fu
It seems, because of cgstm8 crash, the file is incomplete.
I have tried every options with cpstm8 and cgstm8 but, it seems their is problem with cgstm8 file.
can anyone help,
2018-08-09 6:49 AM
cosmic compiler support as found out the problem with code generator, and following is the reply from them, now the problem has been solved.
Dear Sir,
The problem has been identified on lines 6935 and 6970. The following construct:
timer_data[delete_timer_data_count-1].status &= (u8)~status;
crashes the current code generator when combining an @eeprom index array with the &= operator.
The problem will be fixed in a next release and in the meantime, you must use an auxiliary pointer in such a way:
{
u8 *p;
p = &timer_data[delete_timer_data_count-1].status;
*p &= (u8)~status;
}
We hope that this will help.
Regards,
STM8 Team
COSMIC Software France
Supporting Embedded Innovation since 1983
Tel : +33 (0)1 43 99 53 90
Fax: +33 (0)1 43 99 14 83
Web site: www.cosmicsoftware.com
P Only print this mail if necessary
P Afin de contribuer au respect de l'environnement, merci de n'imprimer ce courriel que si nécessaire
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.