Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

EVSPIN32F0601S1 not running motor

Hi All,I am trying to get up and running the above hardware. I downloaded the software for the board, and we already use IAR compiler here. After compiling and downloading (via the STLink), the system runs the program just fine.However, I just need t...

Efficiency and Power Dissipation of HFDA801L

We would appreciate it if you could provide information regarding the changes in efficiency and power dissipation (thermal performance) of the HFDA801L under the following conditions:Device: HFDA801LSupply Voltage: 14.4VInput Signal: TDM Fs 48kHzLoad...

Nobu3 by Associate
  • 505 Views
  • 1 replies
  • 0 kudos

Resolved! STM8L151G3 TIM4 not working

MCU: STM8L151G3U6ISSUE: TIM4 interrupt doesnt seem working Connections:                 1. LED on pin PB0                 2. Push button/ switch on pin PC5Scenario:1. User press the push button2. Toggles the LEDObservation:Without using the TIM4 inte...

zin10 by Associate II
  • 2508 Views
  • 1 replies
  • 1 kudos

Resolved! Set STEVAL-PROTEUS to USB-MSC

Hi!I have the STEVAL-PROTEUS with FP-SNS-DATAPRO1 v1.1.0 programmed on it.Everything works now as expected, except this: Once I completed a sensor acquisition, I cannot configure the board to a mass storage device to retrieve the data file on my PC. ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.