Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LCD registers doesn't updated properly after wake up from active-halt mode in STM8L152R6 and STM8L052C6

I am using STM8L152R6T6 and STM8L052C6 for my project. The code wakes up from active-halt mode by RTC wake up interrupt. There is some LCD display memory (LCD_RAM) updates in RTC wake up interrupt routine. The CPU executes this update function and so...

Hello every one ! i used a low Energy Wireless system-on-chip ( BlueNRG-1) in this application i used 3 input as analog. If i program just 1 input, its works. The problem is when i configure 3 inputs. Can you help me please?

Hello every one !i used a low Energy Wireless system-on-chip ( BlueNRG-1)in this application i used 3 input as analog (ADC1, AD2 and internal VBATSSENS). If i program just 1 input, its works. The problem is when i configure 3 inputs. In fact, when i ...

Aoruc.1 by Associate II
  • 867 Views
  • 0 replies
  • 0 kudos

Which Debugger/Programmer supports ST UPSD3234 ?

We have a very old product that was developed using upsd3234 MCU. Which Debugger/Programmer supports ST UPSD3234 ?ST Flash Link [FL-101D] programmer was used then and i couldnt find any reference to it anywhere online.Which of the current debuggers c...

Level translator ST2349A is now obsolete

Hi,Level translator ST2349A is being used in one our product which has been qualified and is in production. We like to know alternate part with equivalent footprint and electrical and environmental specification. The best is if we have an option to b...

ckesa.1 by Associate
  • 875 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.