Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.
Hi , i try to run the CLK example from STM8L15x_StdPeriph_Examples, but i can't compile the project successfully , below is my procedure, can you help it?create a new workspace using STVD tooladd the source and head files from the STM8L15x library f...
Hi :)So I've been using the lovely software provided by ST, called ST Visual Develop, which is, not only one of the worst IDE I have ever encountered (I quickly switched to writing the actual code in another editor), but also is full of so many bugs....
the STM8 bootloader manual (UM0560 rev10) appendix B describes fewer families/bootloader versions than the erase/write RAM routines bundled with the FLASHER-STM8 v2.8.0. Specifically the newer BL versions v2.4 and v1.4 are missing, as well as the 256...
Hi,We have the STB6100 Tuner in our products, many of them are in the field.Lately we have been working on a bug in which the STB6100 cause an arbitration lost in the I2C interface.It seems that writing some specific values to the registers cause thi...
I'm helping a friend fix his battery charger. The Micro processor in it is a ST6200. Its spec has a list of Application Notes including the AN433. But a search of the ST web site failed to find it - which seems odd. Any assistance will be appreciated...
hi friends i asked my question just a few days ago but nobody answerd i dont know what should i do when i configure micro controller for cco output it generates out put of course its a little unaccurate when i check that is cco stable by checking CCO...
My CAN Network is working with 500kbps, One if the ECU had SJW(Synchronisation Jump Width) setting as 2 TQ(Time Quanta) whereas other ECU’s in Network had SJW setting as 3TQ. Will such CAN network work ? What is impact on ECU having SJW setting as 2T...
Why did Viper113XS removed from eDesignSuite?Is there a problem about IC? I need to know that because I made a design and ordered the IC, if IC has some problems I need to change it.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.