Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! RoHs data is required

M95256-DRDW8TP is in use.Other RoHs DoC, CoC, or TestReport is required because the customer does not recognize msds' declaration as a RoH declaration in the document on hazardous substance registration. Please make a request. The quantity of parts r...

sungmin by Associate
  • 318 Views
  • 1 replies
  • 1 kudos

Problem with L6566B in flyback power supply

Greetings. I am building a 24V, 240W power supply with the help of the ST eDesign Suite website. The problem I have is that before starting, it goes into a blinking mode. To start it, I have to measure with a multimeter on the ZCD pin. Then, suddenl...

MIInge_8 by Associate II
  • 872 Views
  • 3 replies
  • 0 kudos

TDA7498ETR missing data

I have to say I am unimpressed with ST's tech support (there is none: they just referred me to the forums).  And when I selected the 'Analog and audio' group, I couldn't post there as it was 'read-only'!!  If there's a more appropriate product forum ...

Resolved! M24C04-F DNF5 & UFDFPN8 I2C addresses

Dear All,I would like to confirm that two M24C04-F, one in a DNF5 package and one in a FDFPN8 cannot be used together on the same bus. Is that correct? To provide some background, we are using M24C04-F DNF5 but there is a need to add another EEPROM o...

MMici1_0-1762772464920.png MMici1_1-1762772636677.png
MMici.1 by Associate III
  • 578 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.