Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I am getting following error when I try to flash stm8af5288 using stm8gal: in 'bsl_sync()': wrong response 0x00 from BSL.

Hi STM Team,I am trying to flash STM8AF5288T from iMX8MM using stm8gal tool using SPI interface. I successfully cross compiled the stm8gal for Android and run it in the device. It is giving following error:It seems like issue with bootloader. Kindly ...

0693W00000QLGT5QAP.png
H_H_11 by Associate II
  • 1156 Views
  • 0 replies
  • 0 kudos

M24256: Memory addresses I2C

Dear ST-Community,this is my first post, so: Hello!I am currently struggling with a M2425 256kbit Eeprom that i want to address via I2C. I2C-access is working and i can read and write.The part i do not understand is the addresses of the memory. The E...

TWint.2 by Associate
  • 1894 Views
  • 1 replies
  • 0 kudos

STM8AF5288T flashing using iMX8M via SPI protocol

Hi STM8 Team,We have to flash STM8AF5288T MCU via SPI protocol from iMX8M Mini running on Android 11 OS.I have read the AN2659 document to study about IAP and understand the custom bootloader code.I have few queries after reading it which are as foll...

H_H_11 by Associate II
  • 1329 Views
  • 1 replies
  • 0 kudos

Resolved! How to generate .bin file from STVD

Hi STM8 Team,I can see STVD generates .s19 , .sm8 files. I want to generate .bin file. I had tried it by adding the following line in Post-Build section:chex -o $(OutputPath)$(TargetSName).binBut this did not work. Could you please guide me on how to...

H_H_11 by Associate II
  • 3409 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.