Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Is STM8 recomended for beginners?

I have experience with PIC and AVR microcontrollers, but they lack the good debug features of the STM8 series. Furthermore, these microcontrollers aren't cheap. While looking for simple and inexpensive chips, I keep coming across the STM8 series.Mast...

rabbi141 by Associate
  • 7225 Views
  • 30 replies
  • 29 kudos

STM8L052 external interrupt issue?

STM8L052XX – External interrupt on same pin number with different ports (PC0 & PF0)I am using STM8L052R8T6.I have already configured an external interrupt on PC0 (PORTC, pin 0).Now I want to configure an external interrupt on PF0 (PORTF, pin 0) as we...

Glodhi by Associate II
  • 414 Views
  • 1 replies
  • 1 kudos

Resolved! M95P16I write cycle calculation?

I'd like to know about the write cycle for the m95p16i EEPROM.I'm using "Page write (02h)" to write 32 bytes to page 0.The first write is to address 00h, the second to address 21h.I continue to write 32 bytes at a time, writing 16 times until the las...

STM8S103f3 interrupt

Dear ST team, STM8S103f3   I need to initialize interrupt but how I can define particular pin of the port for interrupt .Or how to initialize two interrupt in one port.please share example or library   RM0016thanks and regardsGuddu  

Glodhi_0-1767244137138.png Glodhi_1-1767244178968.png
Glodhi by Associate II
  • 662 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.