Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STUSB4500 GUI did not work if I2C bus have 0x00 ack initially during bus scan. can GUI choose which address to talk to?

I have a design with STUSB4500, and some other I2C devices on the same I2C bus. The GUI works well with the nuclreo F072RB kit, if just fit STUSB4500 device only.once added other I2C devices on the I2C bus as STUSB4500, it always retured no ack at de...

HChen.22 by Associate II
  • 1824 Views
  • 2 replies
  • 0 kudos

Resolved! STiD135 EOL

Hi,Can you tell me if STiD135 is EOL for now?Is there any alternative from ST?Thanks,Christie

CSu.12 by Associate II
  • 6544 Views
  • 7 replies
  • 0 kudos

ST Visual Develop

Hello, everyone,I have a problem with ST Visual Develop, version 4.3.12 (See attachment 1)If I launch ST Visual Develop as administrator, I am not allowed to enter debug mode, but I get the message: "** Connection error (usb://usb): gdi-error [40201]...

Resolved! STM32F103C8T6 blue pill CAN does not work

I'm trying to send CAN messages with the STM32F103C8T6 microcontroller (blue pill hardware with genuine ST chip) to a CAN analyzer without success.I'm using STM32CubeIDE v1.12.0. I double checked the hardware, I'm using PB8 and PB9 pins to connect to...

GRosi.1 by Associate
  • 14898 Views
  • 12 replies
  • 0 kudos

Resolved! SD Card Alternatives

I'm trying to find an embedded solution to replace an SD Card.Basic non-volatile memory, I2C or SPI read/writes.I spotted ST NVRAM, but can't seem to find much about it - is this a new or discontinued product?Are there any other options that I should...

BenG142 by Associate II
  • 4654 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.