Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H407ve FSMC with SRAM

Hi,I'm trying to set up STM32F407Ve (ST Blackboard) FSMC with SRAM 16 bits of data and 10 bits of address on STM32CUBEIDE. However, all I get on the list :LCD Interface, Muxed NOR flash, and MUXE PSRAM.How can I enable SRAM ? 

BEKABEN by Associate II
  • 1144 Views
  • 1 replies
  • 0 kudos

Resolved! STM8S103F remapping timer 1 chan nel 1 to output C6

Hi, I bought me some STM8S103F3 small developent boards from china. Nice stuff. But I would like to make timer 1 channel 1 generate a PWM signal on output C6. This needs some remap of the timer 1 peripheral. Therefore I managed to set the AFR0 bit in...

sthvw by Associate III
  • 2659 Views
  • 2 replies
  • 0 kudos

Intelligent power module

*Is it possible to utilize just one phase from the SLLIMM high-power IPM, which is a 3-phase inverter with a 650V short-circuit rugged IGBT rated at 50A? Additionally, do you have an IPM comparable to the discontinued STGIPS40W60L1, a half-bridge IGB...

Resolved! crtsi.s file startup script for stm8A

Hello all. I am looking for an example startup script to perform a few initialization tests.I came to know that in  https://usermanual.wiki/Document/CXSTM8UsersGuide.1100875490.pdInitializing data in RAM section there is a startup script.I would like...

raja1 by Associate II
  • 2926 Views
  • 2 replies
  • 0 kudos

command line for the utility STVP_CmdLine.exe

Hi, can you please help I am programming my board using STVP_CmdLine.exe utility with the following arguments -ProgMode=SWIM -Device=STM8S105x6 -FileProg={FW_PATH} -verif -no_loop. I need an argument to change the frequency, something like Freq=1800....

Desultor by Associate
  • 1913 Views
  • 1 replies
  • 0 kudos

Resolved! Getting started with the STUSB4500QTR

I'm trying to get started with the STUSB4500QTR and at this point have not changed anything in the device but at the same time I am not using any of its capabilities. The attached schematic shows where I am now. The intent is that a PC (right now jus...

DavePfz by Associate III
  • 4578 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.