Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

M24M02-DRCS6TP/K

Hi, We are currently working on retimer board for internal purpose, we are using M24M02-DRCS6TP/K EEPROM IC in our design. Actually we are facing difficulties in choosing device slave address.  In below attached image, how to choose the MSB address b...

Vishnupriya_0-1695646349200.png

MCU Selection - SD24 + Load Cell

I need help with MCU Selection.The main aim is to replace (STM8s and HX711) Chips in a weight scale project.So, the MCU should be low in cost, include an SD24 with PGA Gain 128.It also should include SPI interface.Note: Load cell maximum weight could...

Sadeen by Associate
  • 1796 Views
  • 2 replies
  • 0 kudos

CR95HF - RFID Click SPI communication issue

Hi,I'm trying to read the UID of an RFID tag (ISO14443A) using an RFID click (CR95HF). Click board is communicating with PIC18F46Q43. I tried to use an example provided by the MPLAB MCC code configurator. The problem from the beginning is that the fu...

msmiha by Associate
  • 1025 Views
  • 0 replies
  • 0 kudos

STPS24045 - Product specifications

Hi Team,I would like to know the Part #STPS24045 is qualified AEC. If not, can you help me to get the Diode with a higher current rating (min: 220A of forward current) and AEC qualified. Thanks, in advance.-Gopi

Gopi-N by Associate
  • 1356 Views
  • 1 replies
  • 0 kudos

Missing ZKW HaMOn Database Data

Dear Sir/MadameConcerning to our ZKW HaMOn (Hardware Management Online)Database, due to our customers' requirements, we need to have some information.Could you please mail me as soon as to send table with MPNs to have required information.Thanks for ...

Somebody know this ic?

Hi again to everyone!I want to know, if somebody know something about this ic´s in the attached pictures (one it´s labeled: "a34 2248", and the other is: "2057 wow1", both in smd structure).It is used to switch  beetwin two hdmi signals.I´ve searched...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.