Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Serial EEPROM SPD ST:M34E04B-FMC9TG

SGS report indicates Test sample: LEAD FRAME; Item no.: C7025-UPG RT, the substance normally include Cu/Ni/Si/Mg, but according to M34E04B-FMC9TG material Composition Declaration file, the substance include Cu/Fe/Zn/FeP, please advise if the substanc...

image.png
Hillary by Associate II
  • 1427 Views
  • 1 replies
  • 0 kudos

marking code

I have an SMD component, with the marking code WBCBR and it's a MOSFET, but I can't find the data sheet, can you help me?

EDLA by Associate
  • 5694 Views
  • 5 replies
  • 0 kudos

EMIF03-SIM02M8 VDD, GND pad connections

Hi, I have two pin connection questions, related to EMIF03-SIM02M8: 1) Are VDD pins 1 & 8 connected internal to the chip or should be connected together externally?2) Pin 9, GND does it have to be connected to system ground, or that's optional?Any la...

AVigh.1 by Associate II
  • 1493 Views
  • 1 replies
  • 0 kudos

Resolved! Questions about LSM6DSO and LIS3MDL in mode 2

Hi, I am trying to build 9 dof imu using LSM6DSO and LIS3MDL, using i2c to write and read lsm6dso and lis3mdl. I am testing the ICs in Raspberry Pi MCU. I am also using sensor hub on LSM6DSO to read/write LIS3MDL.I have two questions that I need help...

el659 by Associate III
  • 1595 Views
  • 1 replies
  • 0 kudos

Marking ID

I am trying to confirm the marking ID on the physical part (4FFT 8311) UFDFPN-8 EP for St. Micro # M24C64-FMC6TG

SJCU by Associate
  • 2832 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.