2016-01-08 5:06 AM
is it possible with the stvd to attach / connect only to a already running target via swim?
#swim #stm8 #attach2016-01-13 4:13 AM
I'm not using STVD, but in general, STVD is more complete than the free tools. With the free stm8flash, I can attach to a running target to write a new program into the flash memory via ST-Link or ST-Link/v2 anytime. So I guess it will work fine with STVD.
PhilippWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.