2005-12-18 11:17 PM
2005-08-24 10:57 PM
Dear ST7 community,
I have found a wrong assembler behaviour when it deals with address evaluation inside a #IF2 directive. The error does not impact on the code generation but only in the test I use to check that some code or data belongs to the same page (see attachment test.txt). When I disable these tests (by commenting them out), the listing file (see attachment list.txt) shows that they are fulfilled (i.e. all of them is in $F0 page) When I enable them, the assembler complains STMicroelectronics - Assembler - rel. 4.48 ERROR: CHECK crosses the SCI Parser page! 1 error on assembly of 'C:\uDev\SW_Projects\uAntHill\pclink.asm' C:\uDev\SW_Projects\uAntHill\pclink.asm(494): as2 : Error 8: End of Assembly while in ENDIF! '' Perhaps I miss some detail of assembler pass #2, or there is a better way to implement my check, but I can not feel safe without a such test in my code... Thank you in advance EtaPhi PS: my experiments have also shown that the #LOAD directive causes problems with the addresses management, since it seems that sometimes the labels addresses that follow them are not correctly computed. ________________ Attachments : List.txt : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0HT&d=%2Fa%2F0X0000000bWa%2FFiK60.ouZIc3dVUTqDxWLfUmSVn86uMsHtzCkIxKf6g&asPdf=falseTest.txt : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0HO&d=%2Fa%2F0X0000000bWX%2FjOPqKPis.thKqb70yCSWvrW0TqMJ8ui_qwBeOITIBSg&asPdf=false2005-12-18 11:17 PM
I found that the source of my problems is my misunderstanding of the assembler documentation.
The st7 assembler reference tells that during the building process the assembler is called twice: before and after the link step. I erroneously thought that these steps are related to the assembler passes, i.e. IF2 is true when the assembler is called after the linker. This is not true, pass 1 and 2 are internal assembler steps that are always executed. To put in effect my test, I changed the #IF2 into #IFDEF DO_TEST and added -d DO_TEST in the assembler command line. This required an hack to the .stp file, since the post-link property page in the project settings is read-only. Is there a ''clean'' (and safe) way to do this? Thanks EtaPhiWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.