2009-04-10 12:30 AM
2009-04-09 2:15 AM
I'm working on a STR730-ks eval board by IAR SYSTEMS. IAR Embedded Workbench IDE rel. 5.30.2.
I'm using the example made by IAR. My question is: all examples that use interrupts work setting ARM C Code mode only (never in Thumb). Which is the reason of this? Is it possible to set Thumb C Code instead of ARM in application where interrupt are used)? How? Where do I must set instructions in order to do this? Thanks Paolo2009-04-09 6:10 AM
arm7/9 always enter isr's in arm mode.
you can switch to thumb mode once you are in the handler. This is why many people use asm to wrap a 'c' interrupt handler. Cheers sjo2009-04-10 12:30 AM
Thank you sjo!
I found solution to my problem enabling ''Generate interwork code'' inside project options of IDE in C/C++ Compiler section. This allows me to mix my Thumb code with Arm Interrupt service routine. Cheers PaoloWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.