2021-12-17 12:34 AM
any inbuild NFC , BLE and Wifi Available in STM32 Controller . or NFC and BLE like that any combination is available ? Please suggest the MCU .
2021-12-17 12:56 AM
Welcome, @SKaru.5, to the community!
There are currently several STM32 with built-in BLE, also a ready-to-use module including an antenna.
Currently an external module is required for NFC because there are too many combinations that, depending on the function, also have to provide high transmission power.
Regards
/Peter
2021-12-17 2:52 AM
for BLE: STM32WB
2021-12-18 3:55 AM
Thanks for your Reply.
if we select STM32WB for BLE and for NFC Interface any Evaluation Board is available .
NFC - P2P and Reader/Write Mode
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.