2008-06-02 5:05 AM
Again on RCCR and oscillator problem with ST7Lite19
2008-04-28 2:22 AM
Hi,
I use ST7LITE19 and 29 with programmer Indart STX. I dont understand how can program without delete EEPROM[0](in eeprom[0] there are factory setting of oscillator)! Now I program with option byte: >write protection: off >read out protection: on and I use Auto program: >Erase option >Erase Code >Blanck check code >Program code >Verify Code >Erase Data >Program Data >Verify Data >Program Option >Verify Option >Run In my program use for initial peripherics: EECSR = 0x00; /* read eeprom */ RCCR = ((EEPROM[0] & 0xFF00) >> 8); but the eeprom[0] is already deleted!!!! :-[ I have try to re-write in sector zero of eeprom with: EECSR |= BIT_1; /* E2LAT = 1 */ EEPROM[0] = 0x6800; // example value 0x6800 EECSR |= BIT_0; while (EECSR & BIT_1) { RefreshWatchdog(); } but when I go to read I found alwais XX in address 0. My error is setting ''Erase Data'' in option byte? I can controll the value in eeprom[0] if I dont lock ''read out'' bytes? Thanks!2008-05-05 12:30 AM
I have found! :D
If I program a microcontroller with ''Read Out Protection'' already setting in ON the eeprom is erased! If I program a microcontroller with ''Read Out Protection'' already setting in OFF the eeprom is untouch. In my Indart STX I must DE-select: >Erase Data >Program Data >Verify Data If I have deleted the first 2 byte of eeprom I can re-write the correct value (measured with oscilloscope) with: EECSR |= BIT_1; /* E2LAT = 1 */ EEPROM[0] = 0x6800; // example value EECSR |= BIT_0; /* E2PGM = 1, start write */ while (EECSR & BIT_1) /* wait for end */ { RefreshWatchdog(); } If EEPROM[0] contains the correct value I can use in my initial peripherics function: EECSR = 0x00; // E2 in read RCCR = ((EEPROM[0] & 0xFF00) >> 8); Never I must to re-program microcontroller locked in Read Out Protection!!!2008-06-02 5:05 AM
I have had the same problem, I wanted to protect my code and set the ''Read out protection'' flag.
When I wanted to install new software I had to erase the device and to my surprise it erased the calibration data, surely this is a bug. I was using the Softec Datablaze Software.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.