2003-09-08 2:39 AM
2003-09-05 8:01 AM
Hi to all,
can you send me some example about ADC temperature conversion with 10bit ? To reduce space I have thought to use a 256 step temperature conversion table (255=100° 0=0°) , not 1024. Is possible ? Many tanks to all mbks2003-09-08 2:39 AM
I think selecting the range will depend up on your type of thermistor you are using. It is because you may have variation of more than 255 steps when the tempreture will rise from 0-100 degrees because of large change of resistance of thermistance so the input voltage with tempreture.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.