2004-02-25 3:57 AM
2004-02-25 1:06 AM
Hi,
I work on ST10F168 and i use 2 64K*8bits SRam chip like one 64K*16bits Sram chip. My problem is that i don't understand to use BHE and A0 signal. I find 2 configurations : 1) WR signal on WR of first chip BHE signal on WR of second chip CS1 on CS of 2 chip Adress A1->A16 on A0->A15 of 2 chip First chip data : low (POL) second chip data : high (POH) 2) WR signal on WR of 2 chip BHE signal on CS on first chip A0 signal on CS of second chip adress P1H on A8->A15 of first chip adress P1L on A0->A7 of second chip First chip data : low (POL) Second chip data : high (POH) So, i don't see the difference between the 2 configurations ! If someone can explain to me the differences or advantages......... Thanks regards, Jim2004-02-25 3:35 AM
Hello.
In the St10 BUSCON register you have a lot of configurations possible. And it is also related to the SYSCON regsiter bit 7: WRCFG. With this bit you select the way the pins /WR and /BHE are working. 1/ If WRCFG = 0, you have the pin /WR = write and /BHE = byte high enable This corresponds to your configuration 2 below. The /WR signal is always connected to the 2 SRAMs. When you need to perform an 8 bit access, ''chip select'' will enable the correct SRAM. For the high byte, the chip select signal is /BHE, for the low part it is A0 address line. 2/ If WRCFG = 1, the pin /WR is the signal /WRL = write low and the pin /BHE is /WRH = write high. This corresponds to your configuration 1. The CS always enables both SRAMs but for 8 bit write access only 1 SRAM get an active write signal. The selection between the 2 modes depends on the SRAM you have because the timings are not the same in the 2 cases: check the need of your SRAM with regard to CS active before/after Write signal. Have a look to the datasheet AC timings part where you have chronograms for the signal. Also your configuration 2 can not be used if you have several devices on the external bus because the SRAMs may answer for any read/write action as the chip select in not based on a window range. I hope I helped you. Regards, Kenshin2004-02-25 3:57 AM
thanks for your precision !
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.