2021-10-12 4:10 AM
hi, am doing a keyword spotting in SensorTile_Box. I have done TFlite model and analyzed in MX tool, generated C code. Now, I want to know where the execution takes place. I want to use LED when it recognizes the voice. But, I didn't know where to write the code led to respond to voice.
Can you help please?
Regards,
shankari
Solved! Go to Solution.
2021-11-05 7:51 AM
Hi shankari,
You might start from a sample project/code, for example the FP-AI-SENSING1 function pack, that supports also projects running on the Sensortile.box.
You can find some examples in \Projects\STM32L4R9ZI-SensorTile.box\Applications\SENSING1 folder.
In particular, middleware libraries generated thanks to STM32CubeMx extension called X-CUBE-AI featuring example implementation of neural networks for real-time:
You need these files:
The green LED can be simply managed toggling the proper GPIO (e.g. the PF2 for the green led), as shown in the schematic below.
-Eleon
2021-11-05 7:51 AM
Hi shankari,
You might start from a sample project/code, for example the FP-AI-SENSING1 function pack, that supports also projects running on the Sensortile.box.
You can find some examples in \Projects\STM32L4R9ZI-SensorTile.box\Applications\SENSING1 folder.
In particular, middleware libraries generated thanks to STM32CubeMx extension called X-CUBE-AI featuring example implementation of neural networks for real-time:
You need these files:
The green LED can be simply managed toggling the proper GPIO (e.g. the PF2 for the green led), as shown in the schematic below.
-Eleon
2021-12-31 10:48 AM
Hello,
I face a very similar challenge: the asc_data.c holds the inference matrix, e.g.
How can I generate an inference that suits the same release used in FP-AI-SENSING1 ?
I have a two-class model inference.
Thanks,
M
2022-01-03 10:44 PM
its better to use 3-classes, since the function pack they have used 3 classes-( indoor, outdoor and vehicle).
Can you tell me what is the duration of the dataset u have used?
Are you using the same Python script for the model creation which ST use?
If you want match exactly with the function pack, I think you have to used the same python script by changing the classes.
Also, use the exact version which they used in function pack.
Keras---2.2.4
Tensor flow---1.14.0
Librosa---0.8.0
STM32MX CUBE- 5.0
X-CUBE AI-4.1.0
Thanks,
Shankari
2022-01-03 10:47 PM
Also, its better to use TFlite models to match with the inference matrix.
2022-01-11 6:32 AM
Hello Shankari,
Thanks for your suggestions. I use a dataset of 5-sec-long audio recordings.
I have used the same Python script available in FP- AI-SENSING1, but I realized a two-class NN.
Did you ever test Wavelet scattering for audio signals ?
Regards,
Marco
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.