2018-06-15 8:12 PM
We are seeing a large current draw when the LSM6DSL is in power-down mode, or low-power mode. The current measured is roughly 120 uA. IC is wired for I2C. We have an identical setup with a LIS3DH that does not have this issue.
Is there a register we need to change? Again , this 120 uA appears when power is supplied to the IC.
LSM6DSL Connections:
SDO: Unconnected
SA0: Unconnected
SDx:
Connected to
GroundSCx:
Connected to
GroundINT1: Floating
INT2: Floating
CS: External pull-up with 10k
SCL: Connected to MCU i2c lines and other I2C devices - External pull-up with 10k
SDA:
Connected to MCU i2c lines and other I2C devices - External pull-up with 10k
#power-consumption #lsm6dsl2018-06-18 3:09 AM
SA0 cannot be unconnected.
It must be connected to GND or VDDIO.
2018-06-18 7:50 PM
Hi Miroslav,
Thank you for your reply. Could you elaborate ? The IC works fine with SA0 floating. Are you saying that extra current is drawn when this pin is left floating? If so, why is the documentation not more explicit ? Or did we miss something?
Would enabling this pull-up help?
'Default: Input without pull-up. Pull-up is enabled if bit SIM = 1 (SPI 3-wire) in reg 12h.'
Thanks again for your help, much appreciated.
2018-06-19 9:24 AM
You can try to enable SPI 3-wire in reg 12h or try to connect the SA0 pin to VDDIO or GND.
If it will not help, please share your schematics.
2018-06-22 5:17 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.