2022-05-18 1:55 AM
Hello,
I'm working on the "STEVAL-MKI182V2" mounted on the "STEVAL-MKI109V3" development board. Initially, I downloaded the Standard c Drivers from the following link "https://github.com/STMicroelectronics/STMems_Standard_C_drivers" where I found the ".ioc" file called "_prj_MKI109V3" which is specifically developed for the MKI109V3 board.
Then after I have added the "ISM330DLC" driver files and example code called "ism330dlc_read_data_polling.c" from the following link "https://github.com/STMicroelectronics/STMems_Standard_C_drivers/tree/master/ism330dlc_STdC" after adding I was just calling "ism330dlc_read_data_polling" function in the main while loop.
Now the issue is, after dumping the code I'm not able to read the "WHO AM I" register. Because of that
if (whoamI!= ISM330DLC_ID) while (1); /*manage here device not found */
controller is getting stuck in the above while loop.
Now I really need help because the project is getting delayed and still, we are stuck with this issue for almost 1 and a half months now.
One thing I observed was that after dumping.bin file(from the Unico GUI package) I was able to see the changing data using UNICO GUI.
Here I'm attaching my project zip file below. Please let me know if you can help me with this issue.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.