2021-05-20 12:12 AM
If the vibration range in acceleration of iis3dwb is 39m/s^2 (4g), what is its vibration range in velocity mm/s? Please advise. Thanks!
2021-05-21 3:43 AM
Hi @JTam.1 ,
You can use the standard harmonic oscillator equations to derive the speed value from the acceleration.
Stated that, at the peak, the followings hold:
you get:
and w is the , equal to 2 * pi * freq, where freq is the frequency of interest, for example 1kHz.
The calculation leads to:
These value are close to the ones declared in the UM2566 user manual, that you also reported in this post.
If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster.
-Eleon
2021-07-19 6:25 PM
Hi Elleon,
You said the speed range can attain 6 mm/s. However, I found that the IIS3DWB sensor can measure speed of 16.45mm/s RMS or higher. Why? Please advise. Thanks!
2021-07-20 12:35 AM
Hi @JTam.1 ,
my example was related specifically to a 4g (rms) - 1kHz stimulus.
In order to achieve higher speeds, considering the formula speed = acc / (2*pi*freq), you can act on two parameters:
Hope this can clarify a bit more.
-Eleon
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.