2018-11-04 2:35 PM
The datasheet pin description table Function column simply states “Connect to GND�?. Every other pin in the table has their function described, but “Connect to GND�? says nothing about its function. Is this a reset pin (active high)? If so, can it be used connected directly to a microcontroller, so we can force a hard reset of the chip?
There is also nothing about it in the application notes.
So, what is the function of this pin?
Any help, greatly appreciated
2018-11-05 12:16 AM
Res means Reserved, the pin should be connected to GND it doesn't have any functionality.
2018-11-06 2:31 PM
Thank you
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.