2013-09-07 9:21 AM
What is sensor fusion?
#motion-sensor #inemo #sensor-fusion #sensor-fusion #inemo2013-09-09 9:43 AM
Hello Naue,
Sensor fusion is a software algorithm which uses data from the accelerometer, gyroscope and magnetometer to output information such as quaterniosn, heading, pitch, roll, yaw, linear acceleration and gravity. The user will still have to create their own software application based on these outputs. ST sensor fusion is the iNEMO_Engine which is provided for free when used with ST Motion sensors. For more details please visit Thank you, Thiago ReisFrom: naue
Posted: Saturday, September 07, 2013 6:21 PMSubject: What is sensor fusion?2013-09-12 5:04 AM
I am wondering if there are any plans to offer the iNEMO software libraries with the inclusion of pressure sensors for a ''10 axis'' solution to help compensate for altitude?
Adam2013-09-17 4:39 AM
Currently the pressure sensor is not used in the iNEMO software libraries
because the target of the sensor fusion algorithm is to provide as output the inclination/orientation and angular information.
Thiago2013-09-19 10:33 AM
Do you have the download link for the inemo software libraries?
2013-09-23 9:21 AM
Hello Albert,
To download the iNEMO Software libraries you can access the below link:
http://www.st.com/web/en/catalog/tools/FM147/CL1818/SC1528?s_searchtype=keyword
After that you can choose what is the library version that you are looking for, then you will find a link to contact the ST office responsible for your location, and it will be provided a couple of forms that must be signed and submitted.
Thank you very much, Thiago ReisWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.