2020-08-25 1:16 AM
Hello,
We want to set the ECE threshold of the VL6180x.
We are following the document DT0034 - VL6180X early convergence estimate implementation.
SAMPLE = 119 (reg 0x10A)
MAX_CONV = 15 (reg 0x01C)
PERIOD = 48 (reg 0x10A)
TIME = (SAMPLE + 1) * (24 + 70 + (PERIOD*10)) + 200
TIME = 69080
CONV_TIME = MAX_CONV * 1000 - TIME
CONV_TIME = -54080
Is it possible to have a negative convergence time and how to handle it?
Thanks for your help,
Thomas
Solved! Go to Solution.
2020-08-25 7:50 AM
A while back we had a lot of questions like this. So instead of reading complex manual and trying to figure it all out, we wrote an API that does it all for you.
That API can be found at:
Even if you don't use the API, there is a function in there that will set the max convergence time for you.
And look it over for other routines you might need.
And if you are so inclined - just use the API in your project. All the functions have been validated.
The following is what that API does. Compare it to yours.
good luck
static int VL6180x_RangeSetEarlyConvergenceEestimateThreshold(VL6180xDev_t dev)
{
int status;
const uint32_t cMicroSecPerMilliSec = 1000;
const uint32_t cEceSampleTime_us = 500;
uint32_t ece_factor_m = VL6180xDevDataGet(dev, EceFactorM);
uint32_t ece_factor_d = VL6180xDevDataGet(dev, EceFactorD);
uint32_t convergTime_us;
uint32_t fineThresh;
uint32_t eceThresh;
uint8_t u8;
uint32_t maxConv_ms;
int32_t AveTime;
LOG_FUNCTION_START("");
do {
status = VL6180x_RdByte(dev, SYSRANGE_MAX_CONVERGENCE_TIME, &u8);
if (status) {
VL6180x_ErrLog("SYSRANGE_MAX_CONVERGENCE_TIME rd fail");
break;
}
maxConv_ms = u8;
AveTime = _GetAveTotalTime(dev);
if (AveTime < 0) {
status = -1;
break;
}
convergTime_us = maxConv_ms * cMicroSecPerMilliSec - AveTime;
status = VL6180x_RdDWord(dev, 0xB8, &fineThresh);
if (status) {
VL6180x_ErrLog("reg 0xB8 rd fail");
break;
}
fineThresh *= 256;
eceThresh = ece_factor_m * cEceSampleTime_us * fineThresh / (convergTime_us * ece_factor_d);
status = VL6180x_WrWord(dev, SYSRANGE_EARLY_CONVERGENCE_ESTIMATE, (uint16_t)eceThresh);
} while (0);
LOG_FUNCTION_END(status);
return status;
}
2020-08-25 7:50 AM
A while back we had a lot of questions like this. So instead of reading complex manual and trying to figure it all out, we wrote an API that does it all for you.
That API can be found at:
Even if you don't use the API, there is a function in there that will set the max convergence time for you.
And look it over for other routines you might need.
And if you are so inclined - just use the API in your project. All the functions have been validated.
The following is what that API does. Compare it to yours.
good luck
static int VL6180x_RangeSetEarlyConvergenceEestimateThreshold(VL6180xDev_t dev)
{
int status;
const uint32_t cMicroSecPerMilliSec = 1000;
const uint32_t cEceSampleTime_us = 500;
uint32_t ece_factor_m = VL6180xDevDataGet(dev, EceFactorM);
uint32_t ece_factor_d = VL6180xDevDataGet(dev, EceFactorD);
uint32_t convergTime_us;
uint32_t fineThresh;
uint32_t eceThresh;
uint8_t u8;
uint32_t maxConv_ms;
int32_t AveTime;
LOG_FUNCTION_START("");
do {
status = VL6180x_RdByte(dev, SYSRANGE_MAX_CONVERGENCE_TIME, &u8);
if (status) {
VL6180x_ErrLog("SYSRANGE_MAX_CONVERGENCE_TIME rd fail");
break;
}
maxConv_ms = u8;
AveTime = _GetAveTotalTime(dev);
if (AveTime < 0) {
status = -1;
break;
}
convergTime_us = maxConv_ms * cMicroSecPerMilliSec - AveTime;
status = VL6180x_RdDWord(dev, 0xB8, &fineThresh);
if (status) {
VL6180x_ErrLog("reg 0xB8 rd fail");
break;
}
fineThresh *= 256;
eceThresh = ece_factor_m * cEceSampleTime_us * fineThresh / (convergTime_us * ece_factor_d);
status = VL6180x_WrWord(dev, SYSRANGE_EARLY_CONVERGENCE_ESTIMATE, (uint16_t)eceThresh);
} while (0);
LOG_FUNCTION_END(status);
return status;
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.