2020-08-25 5:39 AM
Hello.
I use STM32L452 mcu, STM32CubeIDE 1.3.1, simple SD card on 1 GB.
I want to connect SD card to mcu, using SD 4 bit Wide bus, but I can't understand how to connect Detect_SDIO pin, because this mode needs all 9 pin.
It is a problem, because I wont to connect it, but get FR_DISK_ERR error.
Could Detect_SDIO absence be cause of FR_DISK_ERR?
Thank you for reading.
2020-08-25 5:54 AM
The socket detect pin can be any available IO pin, typically the socket grounds the pin when the card is inserted.
The DISKIO layer typically flags a NOT READY type error based on the detected state.
2020-08-25 6:05 AM
Thank you for so fast reply.
So, I can connect one by D0, D1... to Detect_SDIO?
2020-08-25 6:11 AM
Huh?
Something like PC3 or PA7, a pin unrelated to the SDIO/SDMMC peripheral.
CLK
CMD
D0
D1
D2
D3
Should have their own connection to the socket.
Card Detect in this context is typically a mechanical switch on the socket frame itself.
2020-08-25 6:51 AM
Sorry, I meaned D0, D1, D2 and D3 in SD card. I also connect SD to MCU directly via wires and pinches. So, can I connect, for example, PA7(Detect_SDIO) to D0?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.