2021-05-31 8:54 PM
I am trying to compute velocity from the acceleration values by configuring the my IIS3DWB vibration sensor at +-4g. The formula I am using to calculate the instantaneous velocity is V(t) = V0 + ʃa*dt.
What I am experiencing right now is a drift in my velocity values, it is just increasing without applying any force, perhaps due to integration error. I am converting a from g to m/s^2 and I am taking dt=1/ODR (26.7kHz) and I am reading the values from 3k FIFO buffer inside the sensor. Can anyone suggest how can I calculate velocity even with near about accuracy, if not full accuracy?
2021-06-15 4:34 AM
Hi @NukulK ,
it is not possible to have a high accuracy with your application.
there is much noise that can make the integral calculation drift and a high precision is physically impossible.
Niccolò
2021-06-15 8:13 AM
Hello @niccolo.ruffini ,
I understand it is not possible to have high accuracy with this approach.
But is there any other approach that you suggest using which I can calculate instantaneous/RMS/Peak velocity from IIS3DWB vibration sensor?
I want to use this for vibration analysis.
Thanks,
Nukul
2021-06-16 7:34 AM
Hi Nukul @NukulK ,
you can try to better identify the 0 motion level with a range of values.
also, are you using a high pass filter?
Niccolò
2021-06-16 8:35 AM
Hi Niccolo,
By zero motion level, do you mean zero-g offset? Also I am using a HPF, so the DC bias is eliminated from the signal.
Thanks,
Nukul
2021-06-18 7:27 AM
Hi Nukul @NukulK ,
by zero motion level I mean the state where the device is still.
when the device is still there is environmental noise that makes the integral drift, but if you put a range of values inside which the device is considered still and the integral is not even computed, you can avoid the drift (but there is a trade-off with precision to keep into consideration)
good for the HPF.
Niccolò
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.