2025-09-17 4:59 AM
Hi,
I'm using IIS3DWB MEMS sensor to get the motor vibration data which will have a bandwidth of 6kHz and need to store it to a 16GB SD card
I'm confused to calculate the data rate, i mean what is the ODR i need to consider?
My calculation is :
ODR = 26667 and 3 axis 6 bytes, which becomes 160kb/s and 12.89GB/day precisely, which is a lot of data for a day
Should i consider the ODR to be 2x times the bandwidth (6kHz in this case)?
Also let me know about the raw data and how can i filter out the 6khz frequency data that i need
2025-09-17 7:57 PM
ODR appears to be fixed here at 26.667 ksps. You can decimate samples after you read them, but the data will have some aliasing due to this. Note that -3dB bandwidth is guaranteed up to 5 kHz per the datasheet.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.