2021-09-10 11:00 PM
I am trying to build custom boards using LSM9DS1, I shot through the data sheet, but the information on these two pins is not clear enough? What is the purpose of these pins(DRDY_M & DEN_A/G)?
Solved! Go to Solution.
2021-09-14 8:28 AM
Hi @VKoga.1 ,
These pins can appear quite not useful, but are used for debug and test mode purposes.
If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster.
-Eleon
2021-09-14 8:28 AM
Hi @VKoga.1 ,
These pins can appear quite not useful, but are used for debug and test mode purposes.
If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster.
-Eleon
2021-09-14 9:37 AM
@Eleon BORLINI Okay, so leave both the pins floating if you want to use interrupt pins.
2021-09-14 9:38 AM
@Eleon BORLINI How are they used for debug & testing purpose? is it not more efficient to just probe the INTx M(or)A/G pins using a oscilloscope?
2021-09-15 6:23 AM
Hi @VKoga.1 ,
This use is internal to ST only, not accessible to the customer.
-Eleon
2021-09-15 7:05 AM
@Eleon BORLINI should I just leave them float/ no connect??
2021-09-15 9:12 AM
Hi @VKoga.1 ,
if you are sure you don't need them, you can leave unconnected. Usually however they are connected to the application processor in case of future needs.
-Eleon
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.