2023-02-04 9:40 AM
One of the critical measurements for the analysis of bridges is the thermal response. The 201/109 combination has an average thermal response in the FFT of 1.5 milli-g - it is slightly frequency dependent, but ignoring that the standard deviation means that below 3.5 milli-g is just Gaussian data. Anything over 3.5 is structural response, statistically speaking. The 3.5 milli-g is higher than other accelerometers we use, do you have some device with a tighter response to thermal?
2023-04-06 3:36 AM
Ciao @Macneacail,
For your application, I suggest you to look at IIS2ICLX and let me know if you need more information.
2023-04-06 8:54 AM
It is 2 axis only, of no use in bridges, but we are testing the 201/109 in 12 locations, so we will know a lot more in 12 months.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.