cancel
Showing results for 
Search instead for 
Did you mean: 

The IIS2DH measures G force so when I move it on my desk I expect to get a reading change on X-axis. However I also get an oscillation on Z axis which I didn't expect. The steady-state on Z is 270 (2G FS). It oscillates between 242 and 316.

RPowe.9.306
Associate III
 
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Eleon BORLINI
ST Employee

Hi @Community member​ ,

Are you expressing your measures in LSB or mg (I suppose mg)?

The device ZRL should be maximum 90 mg, so along Z you should see 1000 mg (Earth's gravity) +-90mg, not 270mg... are you in flat position? Are you applying any HP filters?

-Eleon

RPowe.9.306
Associate III

Hi,

The board is in a flat position. The accelerometer is programmed for 2G sensitivity. Under gravity, I would expect the Z-axis to read 256 corresponding to 1000mg I think. It actually reads 270 which I guess is within tolerance.

My question really, is this:

If the board remains flat when I move it on the desk, I would expect a change of reading in X and Y. However, I get oscillation on Z which I wasn't expecting. As I said, it oscillates between 242 and 316. (That is Z-axis register reading, not mg)

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.