2020-06-12 1:35 AM
I recently acquired a STEAL-STWINKT1. I'm looking to be able to stream all the raw data from all the sensors (Including the ultrasonic FFT) at the maximum sample rate for a fixed amount of time, specified by me, into a csv file. I have tried many of the test program however can't seem to figure out how this is possible. I was wondering whether you could advise?
2020-06-12 5:13 AM
Hi @GSumm.1 , please check this thread if it can be of any help. There are different examples from the FP-IND-PREDMNT1 function pack that may cover your request. Regards
2020-06-12 5:30 AM
Hi Eleon,
Thank you for the reply. I have tried the functions from this pack. What I'm after is a program which just streams all the data from all the senors into a csv file. I've tried FP-IND-PREDMNT1, speficially the BLE project from here and I can stream some data, however, not all the data at once.
Using the STSW-STWINKT01_V1.3.1 I see this possible on the HSDatalog program however, It only seems to stream 2 sensors and I can't find the .json file where i can configure this to all sensors. Likewise, and more preferably (as i can see the raw data directly, rather than interpreting it through a json file), I see this is possible with the Serial_DataLog Program, this program however, doesn't stream the FFT data calculations and I can't locate the file to edit to show this.
Hopefully that makes more sense. Thanks again,
Gav
2020-06-16 1:07 AM
Hi Eleon,
Thank you for the reply. I have tried the functions from this pack. What I'm after is a program which just streams all the data from all the senors into a csv file. I've tried FP-IND-PREDMNT1, speficially the BLE project from here and I can stream some data, however, not all the data at once.
Using the STSW-STWINKT01_V1.3.1 I see this possible on the HSDatalog program however, It only seems to stream 2 sensors and I can't find the .json file where i can configure this to all sensors. Likewise, and more preferably (as i can see the raw data directly, rather than interpreting it through a json file), I see this is possible with the Serial_DataLog Program, this program however, doesn't stream the FFT data calculations and I can't locate the file to edit to show this.
Hopefully that makes more sense. Thanks again,
Gav
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.