2015-07-29 8:05 AM
All:
I have procurred a STEVAL-MKI109V2 and plug-in board STEVAL-MKI142V1 (LPS25H). When I bring up the UNICO ''Cross-platform User Interface for MEMS demonstration kits'', I am able to see that the device is operating, and it has good values. However, can the interface be changed from the default SPI to run as I2C?I would like to do this to evaluate a target board that has been made up with an I2C interface.I realize that I2C may not be an option for the demo, but is it an option?If so, how do I change the UNICO settings to use the I2C option?Regards,Todd Anderson #unico2015-07-31 1:43 AM
I'm sorry. It is no possible change the UNICO settings to use the I2C option.
Regards AntonellaAll:
I have procurred a STEVAL-MKI109V2 and plug-in board STEVAL-MKI142V1 (LPS25H). When I bring up the UNICO ''Cross-platform User Interface for MEMS demonstration kits'', I am able to see that the device is operating, and it has good values. However, can the interface be changed from the default SPI to run as I2C? I would like to do this to evaluate a target board that has been made up with an I2C interface. I realize that I2C may not be an option for the demo, but is it an option? If so, how do I change the UNICO settings to use the I2C option? Regards, Todd AndersonWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.