2014-01-10 11:15 AM
On power-up, does this gyroscope come up in operating, sleep, or power-down mode (i.e., when all SPI peripherals in my instrument are powered up by a common bus, how much is the gyro drawing?
The datasheet says that Vdd may be disconnected (powering off measurement functions) but if Vdd-IO is maintained the (SPI) bus ''is not blocked.'' I assume this means that SDO and SDI are not pulled low by the powered-down gyro. What is current drain from Vdd-IO when Vdd is off?I plan to use this gyro to measure slow (even < 1dps) rotation of an oceanographic drifter. Can you reassure a mere biologist that this is an appropriate device?Thanks!Tom WolcottProfessor Emeritus #gyroscopes2014-02-05 5:20 AM
Hello Thomas,
The L3GD20 is the appropriate device for your project, it has a sensitivity of 8.75 mdps/digit, this means that you will be able to safely monitor 1 degree variations. On the current consumption part of your question, I still need to verify the current consumption for that aspect. Thank you, Thiago REISWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.