2024-03-05 4:52 AM
SPI communication of ISM330DLC with microcontroller fails rarely and randomly. Most of the time, it is observed when it is on a vibrating source. Could you pls give us some idea to know more about this issue and solving it.
2024-03-05 5:33 AM
Sounds like noise could be affecting the signals. How are the chips connected? Perhaps try a slower clock speed an/dor use LVDS signaling if there is significant distance between the two chips. Better shielding may also help.
2024-03-05 5:59 AM - edited 2024-03-05 6:10 AM
More details needed about your setup, environment, etc.
What, exactly, is the nature of the "failures" ?
@Ponmani wrote:Most of the time, it is observed when it is on a vibrating source. .
Loose connections?
@Ponmani wrote:Could you pls give us some idea to know more about this issue and solving it.
So what testing/debugging/investigations have you done so far?
Add diagnostics - eg, UART output - to give insights into what is going on ...
2024-03-05 6:13 AM
@TDK wrote:if there is significant distance between the two chips.
@Ponmani remember that SPI is not designed for going over significant distances - it's designed for comms between chips on a single PCB.
2024-03-05 9:47 PM
Thanks for the response. We have proper shielding with metal conduits for the SPI lines. I doubt if it can be noise, because, if the failure happens it continuously fails for 2 to 3 hours. Then, it auto- fixes itself.
2024-03-05 9:52 PM
This is observed when installed on a remote place, (where i dont have the ability to scope the signals). It behaved very well in the lab environment.
No loose connections expected as the device is perfectly sealed
2024-03-05 9:53 PM
Will try a slower clock
2024-03-06 4:21 AM
@Ponmani wrote:We have proper shielding with metal conduits for the SPI lines. I doubt if it can be noise, because, if the failure happens it continuously fails for 2 to 3 hours. Then, it auto- fixes itself.
How long are these SPI lines? Again, SPI is not designed for going over significant distances
@Ponmani wrote:I doubt if it can be noise, because, if the failure happens it continuously fails for 2 to 3 hours. Then, it auto- fixes itself.
I don't think that follows.
@Ponmani wrote:This is observed when installed on a remote place, (where i dont have the ability to scope the signals)
So what about UART logging? Or logging to RAM?
@Ponmani wrote:It behaved very well in the lab environment
Well, of course it did - in the nice, clean sanitised conditions of a lab!
Did you do any "stress" testing?
Test at extremes of voltage, temperature, etc?
Test resilience against disruption of comms?
etc, etc, ...
2024-03-06 7:03 AM
Suppose master/slave become out of sync by 1 bit due to noise. How are you synchronizing data between master and slave? Examining the data and looking for bit shifts would be my first option.
Really feels like a noise issue.
2024-03-06 7:33 AM
@TDK wrote:Really feels like a noise issue.
Indeed it does.
Words like "fails rarely and randomly" and "behaved very well in the lab environment" point that way ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.