2020-02-25 3:19 AM
I am using STSW-STLKT01_V2.1.1 package Datalog project to program the sensortile. It works perfectly at 200Hz logging acc+ gyro+ Magnetometer data. I disabled all other sensors. However, if I increase the logging frequency to 500 Hz, it work for 5 seconds and shut down automatically. Does anybody know why?
2020-02-25 4:12 AM
Hi @JWu.3 , please consider that a new FW version (2.2.0) is available, you can try with this revision if the issue is solved. Btw, please note that the STSW-STLKT01 package is not optimized to manage higher rates than default, differently from newer platforms such as the STWINKT1, whose data-logging and data management in general is optimized for every ODR. Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.